Climate change is causing an increasing number of heatwaves worldwide, with severe health and economic consequences. On these hot days, things are particularly difficult for manufacturing companies. Not only do the workers have to keep their cool in the production halls while temperatures rise, the heat can also result in machine tool failure.
Machine tools can continue to work with the required accuracy up to certain temperature limits. Excessive temperatures, above all fluctuations in temperature, can cause problems. The machine owners have to contend with an increasing amount of downtime and have to bear the resulting increases in costs. The costs can vary from one industry to another, and may place a heavy financial burden on the operators.