SOFTWARE

FluidMonitoring Software FluMoS Professional The FluidMonitoring Software FluMoS Professional is a software for reading in, displaying and editing data from HYDAC fluid sensors. It enables the simultaneous connection of 16 sensors. FluMoS Professional can be used in conjunction with the sensors of the latest generation with HSI interface (CS 1000, FCU 1000, MCS 1000, AS 1000, FMM, HYDACLab®) and with the sensors that do not have an HSI interface (CS 2000, FCU 2000, FCU 8000).
  • Parameterisation of the devices via sensor dialogue
  • Tabular and graphic online depiction of the measurement values on the PC
  • Saving of log files to the hard drive
  • Depiction of log files from hard drive/floppy disk and backup as graphics file
  • Processing of saved log files, e.g. with Microsoft Excel
  • Update to new release through the Internet
  • Support per E-mail
  • Greater operator convenience
Areas of application:
  • Remote monitoring of the sensor measurement values
  • Condition-based maintenance
------------------------------------------------------------------ FluidMonitoring Software FluMoS Light The FluidMonitoring Software FluMoS Light is a software for reading in, displaying and editing data from HYDAC fluid sensors. It enables the simultaneous connection of 3 sensors. FluMoS Light can be used in conjunction with the sensors of the latest generation with HSI interface (CS 1000, FCU 1000, MCS 1000, AS 1000, FMM, HYDACLab®) and with the sensors that do not have an HSI interface (CS 2000, FCU 2000, FCU 8000).
  • Tabular and graphic online depiction of the measurement values on the PC
  • Saving of log files to the hard drive
  • Depiction of log files from hard drive/floppy disk and backup as graphics file
  • Processing of saved log files, e.g. with Microsoft Excel
  • Greater operator convenience
Areas of application:
  • Remote monitoring of the sensor measurement values
  • Condition-based maintenance
------------------------------------------------------------------ ContaminationControl Software CoCoS 1000 The ContaminationControl Software CoCoS 1000 is available to the user for operating the ContaminationSensors of the CS 1000 series. The user interface of the software shows the display with the control panel of the CS 1000. The devices can be operated easily from the PC with the aid of the CoCoS 1000, and the measurement values can be saved as a file. Please observe the installation instructions. The ConditionSensor Interface CSI-D-5 (HYDAC Mat. No. 3249563) can be used for simple connection of the CS 1000 to the PC. The ContaminationControl Software CoCoS 1000 is available in English. The elements tied to Microsoft are displayed in the language specified in the operating system.   ------------------------------------------------------------------ ContaminationControl Software CoCoS Light The FluidControl Units of the FCU 2000 Series and FCU 8000 Series, as well as the ContaminationSensors CS 2000 with DIN measuring bus output (RS232 and RS485), can be operated conveniently with CoCoS Light. In the case of RS485, an additional RS485/RS232 interface converter is necessary (HYDAC Mat. No. 6013281). Measurement values can be depicted online in either tabular or graphics from with the CS. Measurement logs can be transferred and edited with all FCUs.   ------------------------------------------------------------------ FluidMonitoring Toolkit FluMoT The FluidMonitoring Toolkit FluMoT is a driver package which is used for integrating HYDAC fluid sensors or sensors of the latest generation with HSI interface in the customer's own PC software. FluMoT thus replaces all previous drives (e.g. for Windows, LabVIEW) for the integration of ContaminationSensors and FluidControl Units. The driver package is comprised of the following modules:
  • dll
  • HSI/HeCom
  • DinMessBus
Example programmes
  • Delphi
  • LabVIEW
  • VB/VBA
  • C/C++
  • ONE driver package for ALL fluid sensors
  • Application in the customer's own software
  • Simple example programmes
Freeware for downloading here
  • FluidMonitoring Software FluMoS Light (Freeware)
  • ContaminationControl Software CoCoS Light
  • ContaminationControl Software CoCoS 1000